Hi dav1
yes external usb hub can be connected to i.MXRT1050 usb host.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
1. Just to clarify that we're talking "Multi-Point Support", i.e. that the USB controller when operating in host mode can host multiple USB peripheral devices. Please confirm.
2. How many end-points are supported?
3. Is there a driver or example project available, demonstrating multiple usb-devices running via a hub?
Thanks David
Hi David
number of endpoints is described in sect.55.1.1 Features
i.MX RT1050 Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf
For new questions suggest to create new thread.
Best regards
igor
from the "i.MX RT1050 Processor Reference Manual"
Up to 8 bidirectional endpoints
Although there is no separate Transaction Translator block in the system, the transaction translator function normally associated with a USB 2.0 high speed hub has been implemented within the DMA and protocol engine blocks to support connection to full and low speed devices.
I've created a new topic for item 3: