i.MXRT1170-EVK ethernet example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MXRT1170-EVK ethernet example

跳至解决方案
1,391 次查看
igrinberg
Contributor II

Hi,

I'm trying to find basic example of enet configuration on i.MXRT1170-EVK.

The SDK contains only examples using loopback cable.

1. Is there an example running internal loopback not requiring loopback cable?

2. Is there an example connecting to an external target?

 

Thanks,

Irina.

0 项奖励
回复
1 解答
1,378 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @igrinberg 

Thank you for your interest in the NXP MIMXRT Product, I would like to provide service for you.
Answer your questions:
1. Is there an example running internal loopback not requiring loopback cable?
Answer: I checked the RT1170RM, I find it has the loopback mode, please check it like the following information.

kerryzhou_0-1640672047189.png


 
Updating Media

 

 

But, if you test the SDK, I still recommend to follow the SDK enet project readme to prepare the related cable.

2. Is there an example connecting to an external target?
Answer:you can test the lwip project:
SDK_2_10_1_MIMXRT1170-EVK\boards\evkmimxrt1170\lwip_examples
It can connect to the external target.

Wish it helps you!

Best Regards,

Kerry

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,379 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @igrinberg 

Thank you for your interest in the NXP MIMXRT Product, I would like to provide service for you.
Answer your questions:
1. Is there an example running internal loopback not requiring loopback cable?
Answer: I checked the RT1170RM, I find it has the loopback mode, please check it like the following information.

kerryzhou_0-1640672047189.png


 
Updating Media

 

 

But, if you test the SDK, I still recommend to follow the SDK enet project readme to prepare the related cable.

2. Is there an example connecting to an external target?
Answer:you can test the lwip project:
SDK_2_10_1_MIMXRT1170-EVK\boards\evkmimxrt1170\lwip_examples
It can connect to the external target.

Wish it helps you!

Best Regards,

Kerry

0 项奖励
回复