i.MXRT1170-EVK ethernet example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT1170-EVK ethernet example

Jump to solution
1,259 Views
igrinberg
Contributor II

Hi,

I'm trying to find basic example of enet configuration on i.MXRT1170-EVK.

The SDK contains only examples using loopback cable.

1. Is there an example running internal loopback not requiring loopback cable?

2. Is there an example connecting to an external target?

 

Thanks,

Irina.

0 Kudos
Reply
1 Solution
1,246 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @igrinberg 

Thank you for your interest in the NXP MIMXRT Product, I would like to provide service for you.
Answer your questions:
1. Is there an example running internal loopback not requiring loopback cable?
Answer: I checked the RT1170RM, I find it has the loopback mode, please check it like the following information.

kerryzhou_0-1640672047189.png


 
Updating Media

 

 

But, if you test the SDK, I still recommend to follow the SDK enet project readme to prepare the related cable.

2. Is there an example connecting to an external target?
Answer:you can test the lwip project:
SDK_2_10_1_MIMXRT1170-EVK\boards\evkmimxrt1170\lwip_examples
It can connect to the external target.

Wish it helps you!

Best Regards,

Kerry

View solution in original post

0 Kudos
Reply
1 Reply
1,247 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @igrinberg 

Thank you for your interest in the NXP MIMXRT Product, I would like to provide service for you.
Answer your questions:
1. Is there an example running internal loopback not requiring loopback cable?
Answer: I checked the RT1170RM, I find it has the loopback mode, please check it like the following information.

kerryzhou_0-1640672047189.png


 
Updating Media

 

 

But, if you test the SDK, I still recommend to follow the SDK enet project readme to prepare the related cable.

2. Is there an example connecting to an external target?
Answer:you can test the lwip project:
SDK_2_10_1_MIMXRT1170-EVK\boards\evkmimxrt1170\lwip_examples
It can connect to the external target.

Wish it helps you!

Best Regards,

Kerry

0 Kudos
Reply