i.MXRT Jlink programming with additional binary

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MXRT Jlink programming with additional binary

1,224 次查看
ecorini
Contributor I

Hi, 

I'm using latest 11.7.0 version of MCUXpresso.

Is it possible when debugging a IMXRT with Jlink to load a raw binary in addition to the compilation .axf file?

Thank you very much!

 

 

0 项奖励
回复
5 回复数

1,209 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, so I am reviewing your case, but I understand the next if I do not right, please let me know.

There are 2 forms to get the .bin from the IDE, the first is explained on the next page MCUXpresso IDE: S-Record, Intel Hex and Binary Files | MCU on Eclipse.

The final form is the easiest when you build your project appears a Debug file there in the .axf file click right>Binary Utilities>Create binary.

Pavel_Hernandez_0-1676948875634.png

 

Let me know if you have more questions.

Best regards,
Pavel

0 项奖励
回复

1,201 次查看
ecorini
Contributor I

I need to load an additional binary (not present in .axf file) when i launch Jlink debug configuration.

In PEMicro this option is present in debug configuration:

ecorini_0-1676962286112.png

But i can't find a similar option in JLink debug configuration, and I was wondering if anyone had the same problem.

Thank you very much.

 

Best Regards!

0 项奖励
回复

1,183 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello,

Are you referring to the windows configuration like this?

Pavel_Hernandez_0-1677015185843.png

Pavel_Hernandez_1-1677015292834.png

Sorry, I do not understand could you elaborate further?

Best regards,
Pavel

 

 

0 项奖励
回复

1,171 次查看
ecorini
Contributor I

Yes, with PeMicro i can download an additional binary when downloading the executable.

See option in red in PeMicro debug configuration:

ecorini_0-1677070096299.png

I can't find a similar option in J-Link debug configuration.

The question is:

Is it possible to achieve the same result in some way?

 

Thank you very much.

Best Regards

0 项奖励
回复

1,159 次查看
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I recommend reviewing the information on the MCUxpresso for more details.  Review the chapter maybe could help you 18.5.2 arm-none-eabi-size.

Best regards,
Pavel

 

0 项奖励
回复