i.MXRT 106X CM7_CFGITCMSZ and CM7_CFGDTCMSZ

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MXRT 106X CM7_CFGITCMSZ and CM7_CFGDTCMSZ

525 次查看
dwotherspoon
Contributor I

I'm using an i.MXRT1062 for a project and noticed that between revisions 2 and revisions 3 of the "i.MX RT1060 Processor Reference Manual" the fields in IOMUXC_GPR_GPR14 for TCM sizes were removed. I don't have access to the changelog between these two manuals, can anyone tell me why these fields were removed from the manual?

标签 (1)
0 项奖励
回复
1 回复

484 次查看
PabloAvalos
NXP TechSupport
NXP TechSupport

Dear @dwotherspoon 

 

Please accept our apologies for the delay on our response. I appreciate your patience.

 

Regarding your question, these bits were removed because they are not dynamically changeable.

To set ITCM/DTCM memory to 0 Bytes you can use FlexRAM partition registers (FLEXRAM_BANK_CFG_SEL and FLEXRAM_BANK_CFG in GPR), or blown eFuse (Default_FlexRAM_Part bits in fusemap) if you want to permanently disable them.

 

But be careful the software should avoid touching the ITCM/DTCM by any means when they are 0 bytes.

 

Hope this solve your concern. Please let me know if you have some more questions.

 

Best Regards.
Pablo Avalos.

0 项奖励
回复