i.MXRT 106F OASIS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT 106F OASIS

1,688 Views
yuichiro_yamagu
Contributor I

I am investigating 「i.MX RT Solution For Secure Face Recognition」.

I don't know much about OASIS.

Is OASIS  a machine learning library like Tensor Flow?

Also, could you please tell me Document about OASIS?

 

 

0 Kudos
Reply
3 Replies

1,657 Views
yuichiro_yamagu
Contributor I

Thank you for answer.

0 Kudos
Reply

1,673 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

The algorithms being used for face detection and recognition are using a custom inference engine/architecture we internally call "Oasis-Lite" which is distinct from popular open-source engines like TensorFlow Lite. When a customer purchases the SLN-VIZNAS-IOT they are given access to the source code for the firmware being run on the chip, but the "oasis-Lite" inference engine is provided as a runtime library that cannot be modified by the customer. That being said, we at NXP are continually upgrading and improving the performance and feature set of our engine so that faces can be detected and recognized even faster, and new features can be added. 
 
Regards, 
Victor 

1,414 Views
wuruoyu
Contributor I

I have purchased SLN-VIZNAS-IOT and I am wondering how I can access to the source code of the firmware. Thanks in advance!

0 Kudos
Reply