i.MXRT 1062 custom API based USB to SPI communication

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MXRT 1062 custom API based USB to SPI communication

414件の閲覧回数
nlv20770
NXP Employee
NXP Employee

Hello,

I am currently creating a validation board for a NXP product, on which I want to use a Teensy 4.1 development board. This board is populated with a MIMXRT1062DVL6B.

The goal of the MCU will be to ensure the bidirectional communication between my product (SPI bus) and a PC (USB, maybe later ethernet). I want to implement high level API like commands that will trigger hundreds of exchange with my product, perform ADC conversions and in the end retrieve the data on the PC.

Could you share with me an example / project to help me to start ?

Thanks a lot !

Best Regards,

Gaël

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)