i.MX RT1170 can use Gigabit Ethernet to do MAC to MAC without PHY

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX RT1170 can use Gigabit Ethernet to do MAC to MAC without PHY

跳至解决方案
1,968 次查看
WJC
Contributor I

Hello,

I want to use the Gigabit Ethernet to do MAC to MAC without PHY (RGMII to RGMII) on RT1170.
Does this work?

 

0 项奖励
回复
1 解答
1,892 次查看
danielchen
NXP TechSupport
NXP TechSupport

Yes, ENET 10/100Mbps can use MAC-to-MAC without phy.  But only RMII interface can support it.

 

Regards

Daniel

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,908 次查看
WJC
Contributor I


ENET 10/100Mbps can use MAC-to-MAC without phy.

Attached the simple block diagram.

Thanks in advance.

WJC

0 项奖励
回复
1,893 次查看
danielchen
NXP TechSupport
NXP TechSupport

Yes, ENET 10/100Mbps can use MAC-to-MAC without phy.  But only RMII interface can support it.

 

Regards

Daniel

0 项奖励
回复
1,885 次查看
WJC
Contributor I

Thanks for your reply.

0 项奖励
回复
1,937 次查看
danielchen
NXP TechSupport
NXP TechSupport

@WJC 

 

RT1170 does not support MAC TO MAC connection without PHY.  Because RT1170 doesn't have delay line inserted on rx/tx data sampling capturing path, so timing will not match.

 

Regards

Daniel