i.MX RT1064 XIP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1064 XIP

1,088 Views
ronald_flass
Contributor I

On the i.MX RT1064, can I read/erase/write the on chip flash while executing in place from that flash at the same time?

Labels (1)
0 Kudos
Reply
1 Reply

888 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Ron Flass

Read is possible, XIP is a read operation by itself. For erase and write operations, please check the following links:

mxrt 1050 XIP from NOR 

At the same time it's not possible, because the MCU needs to get out of XIP mode and then made some write commands.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 Kudos
Reply