i.MX RT1064 EVK PCB Files in Altium Format

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT1064 EVK PCB Files in Altium Format

2,589件の閲覧回数
allthepies
Contributor I

Hi,

I have purchased the i.MX RT1064 EVK and would like to examine the PCB layout however I exclusively use Altium and I cannot import the design files which are in Cadence Allegro format.  Would it be possible to obtain a copy of the design files for this PCB in Altium format please?

Thanks,
Shane

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

2,316件の閲覧回数
jaencer
Contributor I

They just send you the original Allegro files.  There is no Altium version.  We wound up re-designing the whole project in Altium.  

0 件の賞賛
返信

2,369件の閲覧回数
sagonzal
Contributor III

I'm in the same predicament, I've started to design a new board based on i.MX RT1064 and I only see Allegro files. We are in need of Altium files please. Kind regards.

0 件の賞賛
返信

2,514件の閲覧回数
jaencer
Contributor I

We need the same thing.  Are such files available?  

0 件の賞賛
返信

2,520件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hello Shane,

I have contacted you via email.


Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:

This thread is continued as a private discussion with the submitter,
NXP support is not following the thread anymore.
-------------------------------------------------------------------------------

2,284件の閲覧回数
azizsobaka
Contributor I

Hello! I am starting a new design using RT1064 and would like to know if there are Altium files for the design? If so can you please contact me? Thank you!

0 件の賞賛
返信

2,320件の閲覧回数
avbot
Contributor III

Hi, we urgently require these files also - please can you message us? Thank-you!

0 件の賞賛
返信

1,764件の閲覧回数
kksakthi
Contributor I
hi anyone received the IMXRT1064 altium file from NXP? Is it's possible to share me?
0 件の賞賛
返信