i.MX.RT1052 - How to connect timer to Encoder for low speed/velocity measurement?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX.RT1052 - How to connect timer to Encoder for low speed/velocity measurement?

Jump to solution
914 Views
Cindy
Contributor III

Hi,

May I know how to connect timer to the encoder for low speed/velocity measurement?

Thank you!

Best Regards,

Cindy

0 Kudos
Reply
1 Solution
902 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

While we currently do not have an example for the RT1050for motor control, you can use as a base the example for the RT1060 in the SDK.

 

estephania_mart_1-1640273154183.png

 

You will need to make sure to add the motor control library in your SDK.

 

estephania_mart_2-1640273206337.png

 

Regards

View solution in original post

0 Kudos
Reply
1 Reply
903 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

While we currently do not have an example for the RT1050for motor control, you can use as a base the example for the RT1060 in the SDK.

 

estephania_mart_1-1640273154183.png

 

You will need to make sure to add the motor control library in your SDK.

 

estephania_mart_2-1640273206337.png

 

Regards

0 Kudos
Reply