i.MX RT 106x SD card voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT 106x SD card voltage

1,484 Views
nickwallis
Senior Contributor I

I'm confused about the NXP i.MX RT 106x reference design SD card voltages

The reference schematics have the option to power the relevant MCU bank from either 3.3V or 1.8V

pastedImage_1.png

pastedImage_2.png

But the SD card connector itself can only be powered from +3.3V

pastedImage_3.png

pastedImage_4.png

... and therefore the card will always output 3.3V levels, and have input thresholds appropriate for 3.3V.

So, how does this even work when configured for 1.8V operation?

regards

-Nick

Labels (1)
Tags (2)
0 Kudos
Reply
4 Replies

649 Views
andrew58210
Contributor II

How is this an error?  SDcards always run off 3.3V even when you change the I/O voltage to 1.8V.18.PNG33.PNG

0 Kudos
Reply

1,380 Views
nickwallis
Senior Contributor I

Hi Felipe,

Thank you for your reply.

So, this looks like an error in the MIMXRT1060-EVK design? And the solution, I think, is that the SD card connector J39 should be powered from NVCC_SD (clearly this will also impact the power switch U37).

The card detect (SD_CD_SW) is OK because it is a switch to GND rather than a driven signal, and it connects to an MCU bank that is powered from +3.3V.

Do you agree?

regards

-Nick

0 Kudos
Reply

1,380 Views
FelipeGarcia
NXP Employee
NXP Employee

Yes, I totally agree with you.

 

Regards,

Felipe

0 Kudos
Reply

1,380 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Nick,

 

Unfortunately, MIMXRT1060-EVK does not support SD card voltage switch due to the limitation in SD card connector that you pointed out.

 

Sorry for the inconvenience this may cause you.

 

Best regards,

Felipe

0 Kudos
Reply