Hello,
We recently moved to imxRT1060.
On trying to run evkmimxrt1060_flexspi_hyper_flash_polling_transfer example runs as following:
"
FLEXSPI hyperflash example started!
Entering the ASO mode
"
There are no further printing as expected.
On debugging it I see that the flash detection seems to be wrong:
flexspi_nor_hyperflash_cfi -> flexspi_nor_hyperbus_read -> fails here !
status_t flexspi_nor_hyperbus_read(FLEXSPI_Type *base, uint32_t addr, uint32_t *buffer, uint32_t bytes)
{
...
status = FLEXSPI_TransferBlocking(base, &flashXfer);if (status != kStatus_Success)
{
return status; <------------ return here
}return status;
}
Can anyone please check this issue ?
Thank you.
ranran
Hi ranran,
On the EVKB-MIMXRT1050 board, the HyperFlash is the default memory and it is required to apply a rework on the board to enable the QSPI Flash, however on the EVK-MIMXRT1060 is the opposite, the QSPI is the default memory and it is required to apply a rework on the board to enable the HyperFlash.
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
It is explained on section 2.6 of MIMXRT1060 Evaluation Kit Board Hardware User's Guide:
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------