connect FLEXIO pins MIMXRT1060-EVKB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

connect FLEXIO pins MIMXRT1060-EVKB

Jump to solution
658 Views
HeritageMarco
Contributor I

Hi, I'm following a I2S EDMA transfer example from the SDK. My problem is that on the readme.txt they say that you need to connect FLEXIO pins to the pad close to J23 as follows:

Captura de pantalla 2022-03-07 a las 7.48.49.png

The problem is that I can't see the way of doing this. Can someone explain how I need to do it?

Thanks in advance.

0 Kudos
Reply
1 Solution
651 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @HeritageMarco ,

This work need a hardware engineer. User should remove R98,R99,R100,R101 and then fly four line from SW5 to  R98,R99,R100,R101's pad. people should solder these lines carefully.

 

Regards,

Jing

View solution in original post

0 Kudos
Reply
1 Reply
652 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @HeritageMarco ,

This work need a hardware engineer. User should remove R98,R99,R100,R101 and then fly four line from SW5 to  R98,R99,R100,R101's pad. people should solder these lines carefully.

 

Regards,

Jing

0 Kudos
Reply