Hi all,
I have had a assert fault issue in ethernetif_drop_frame. It was very intermittent but it occurred once while debugging with J-Link connected so I got some information. This happened because ENET_GetRxBuffer() returned kStatus_ENET_RxFrameFail so that assert occurred at the line of LWIP_ASSERT("ENET_GetRxBuffer() status != kStatus_Success", status == kStatus_Success).
static void ethernetif_drop_frame(struct ethernetif *ethernetif)
{
...
do
{
#if 0 /* Error statisctics */
enet_data_error_stats_t eErrStatic;
/* Get the error information of the received g_frame. */
ENET_GetRxErrBeforeReadFrame(ðernetif->handle, &eErrStatic);
#endif
status = ENET_GetRxBuffer(ethernetif->base, ðernetif->handle, &buffer, &len, 0, &isLastBuff, &ts);
LWIP_UNUSED_ARG(status); /* for LWIP_NOASSERT */
LWIP_ASSERT("ENET_GetRxBuffer() status != kStatus_Success", status == kStatus_Success);
ENET_ReleaseRxBuffer(ethernetif->base, ðernetif->handle, buffer, 0);
} while (!isLastBuff);
...
}
status_t ENET_GetRxBuffer(ENET_Type *base,
enet_handle_t *handle,
void **buffer,
uint32_t *length,
uint8_t ringId,
bool *isLastBuff,
uint32_t *ts)
{
enet_rx_bd_ring_t *rxBdRing = &handle->rxBdRing[ringId];
volatile enet_rx_bd_struct_t *curBuffDescrip = rxBdRing->rxBdBase + rxBdRing->rxGenIdx;
uint32_t address;
/* Check if current rx BD is under usage by certain application */
/* Buffer owner flag, 1: owned by application, 0: owned by driver */
if ((curBuffDescrip->control & ENET_BUFFDESCRIPTOR_RX_SOFTOWNER1_MASK) == 0U)
{
curBuffDescrip->control |= ENET_BUFFDESCRIPTOR_RX_SOFTOWNER1_MASK;
}
else
{
return kStatus_ENET_RxFrameFail;
}
A picture below shows what functions had been called when the assert occurred.
I don't understand why ENET_GetRxFrameSize() returned kStatus_ENET_RxFrameError so ethernetif_drop_frame function was called.
struct pbuf *ethernetif_linkinput(struct netif *netif)
{
...
/* Obtain the size of the packet and put it into the "len" variable. */
status = ENET_GetRxFrameSize(ðernetif->handle, &len, 0);
if (status == kStatus_Success)
{
/* Read frame. */
p = ethernetif_read_frame(ethernetif, len);
}
else if (status != kStatus_ENET_RxFrameEmpty)
{
/* Drop the frame when error happened. */
ethernetif_drop_frame(ethernetif);
}
return p;
}
According to the pictures below, rxBdBase is 0x20000000 (DTC).
I captured the memory data from 0x20000000 as following.
ENET_GetRxFrameSize returns kStatus_ENET_RxFrameError when descriptor's length is 0 or last buffer descriptor's frame has an error. Looking at the memory data above, there shouldn't be the case.
#define ENET_RING_NUM (1U)
#define ENET_RXBD_NUM (10U)
#define ENET_TXBD_NUM (6U)
status_t ENET_GetRxFrameSize(enet_handle_t *handle, uint32_t *length, uint8_t ringId)
{
/* Reset the length to zero. */
*length = 0;
uint16_t validLastMask = ENET_BUFFDESCRIPTOR_RX_LAST_MASK | ENET_BUFFDESCRIPTOR_RX_EMPTY_MASK;
enet_rx_bd_ring_t *rxBdRing = &handle->rxBdRing[ringId];
volatile enet_rx_bd_struct_t *curBuffDescrip = rxBdRing->rxBdBase + rxBdRing->rxGenIdx;
uint16_t index = rxBdRing->rxGenIdx;
bool isReturn = false;
status_t result = kStatus_Success;
/* Check the current buffer descriptor's empty flag. If empty means there is no frame received. */
/* If this buffer descriptor is owned by application, return empty. Only need to check the first BD's owner if one
* frame in mutiple BDs. */
if (0U != (curBuffDescrip->control & (ENET_BUFFDESCRIPTOR_RX_EMPTY_MASK | ENET_BUFFDESCRIPTOR_RX_SOFTOWNER1_MASK)))
{
isReturn = true;
result = kStatus_ENET_RxFrameEmpty;
}
else
{
do
{
/* Add check for abnormal case. */
if (curBuffDescrip->length == 0U)
{
isReturn = true;
result = kStatus_ENET_RxFrameError;
break;
}
/* Find the last buffer descriptor. */
if ((curBuffDescrip->control & validLastMask) == ENET_BUFFDESCRIPTOR_RX_LAST_MASK)
{
isReturn = true;
/* The last buffer descriptor in the frame check the status of the received frame. */
if (0U != (curBuffDescrip->control & ENET_BUFFDESCRIPTOR_RX_ERR_MASK))
{
result = kStatus_ENET_RxFrameError;
break;
}
Can I know why this happen and how to solve this assert fault issue?
Solved! Go to Solution.
This issue was resolved after updating nxp driver and lwip port codes below to the SDK 2.11.1.
This issue was resolved after updating nxp driver and lwip port codes below to the SDK 2.11.1.
Hi,
Thank you for the info.
Plese help to provide which RT product you are using?
Whats the test environments info (IDE/SDK version/EVK board version)?
And please help to guide us how to regenerate this issue. Thanks.
Mike
Hi
Sorry, I thought I had put these information in the post.
[System Information]
I tried to make this issue reproducible but couldn't. This issue is very intermittent and take a couple of days or more. What I can say for sure is that It occurs when there is a lot of connection and disconnection between Modbus Server on our controller and Modbus Client on PC like picture below.
In addition, I can see following messages in our logging.
tcp_input: no PCB match found, resetting. tcp_rst: seqno 0 ackno 1619121200. tcp_input: no PCB match found, resetting. tcp_rst: seqno 0 ackno 2001380479. tcp_input: no PCB match found, resetting. tcp_rst: seqno 0 ackno 3118458873. tcp_input: no PCB match found, resetting. tcp_rst: seqno 0 ackno 1190114352. tcp_input: no PCB match found, resetting. tcp_rst: seqno 0 ackno 1427156108. tcp_input: no PCB match found, resetting. tcp_rst: seqno 0 ackno 3511738084.
I posted another question of watchdog fault issue which is related to this condition, but type of fault is different.
I think that some setting for lwip might have been wrong, however I don't know which part I have to look at.
This assert occurs a little less if increase the ENET_RXBD_NUM value. It was set to 10 and changed it to 20. I think increasing this value whenever such this problem occurs is not a right solution. What other things can I try to solve this issue?
This is a python script. It creates a specified number of threads and each thread create a Modbus client. The Modbus client sends a variable length packet at random cycle time and it automatically connects and disconnects to the server every packet.
number_of_threads = 50
def work(work_id, host, port, unit_id):
client = ModbusClient(host=host, port=port, unit_id=unit_id, auto_open=True, auto_close=True)
for index in range(100000):
number_of_variables = random.randint(1, 50)
cycle_time = random.randint(1, 500)
regs = client.read_holding_registers(0, number_of_variables)
if regs:
print("id:%d:%s" % (work_id, regs))
else:
print("id:%d:read error" % work_id)
time.sleep(0.001 * cycle_time)
# Press the green button in the gutter to run the script.
if __name__ == '__main__':
thread_id = 0
for loop in range(number_of_threads):
thread_id = thread_id + 1
t = Thread(target=work, args=(thread_id, "192.168.3.102", 1502, 1))
t.start()
while 1:
time.sleep(1)