Hi,
When I try to stream 'evkmimxrt1064_dev_video_virtual_camera_freertos' to a Linux machine, VLC fails to open the stream probably due to the following errors (I have obtained them via v4l2 test bench with error logging enabled):
VIDIOC_S_FMT returned -1 (Input/output error)
VIDIOC_S_PARM returned -1 (Input/output error)
Since this is not a problem using VLC on Window, I must assume that ioctl() calls failing on Windows are treated more leniently. I can address this by overriding the error on the device side, but so far I could not find the spot in the USB suit that can bring that about. Can you help?
Hello.
Could you tell me if you are using a virtual machine or a native Linux?
Are these errors from Linux or VLC?
VIDIOC_S_FMT returned -1 (Input/output error)
VIDIOC_S_PARM returned -1 (Input/output error)
Best regards,
Pavel