Hello,
in RT1020 Reference Manual Table 42-3 LPSPI Command Word in Master Mode (continued) is the following entry for FRAMESZ:
Does the above mean if I my frame size is more than one FIFO entry the last FIFO entry should include at least 2 bits of the frame size?
e.g. 32 bits are okay ( = 1 FIFO entry)
33 bits are not okay (= 2 FIFO entries, the second one would only include 1 bit)
64 bits are okay (= 2 FIFO entries)
65 bits are not okay because it would be 2 FIFO entries with 32 bit each and one FIFO entry with 1 bit
Therefore similar frame sizes to 33 bits would be 65 bits, 97 bits, 129 bits, ... Is this correct?
Kind regards,
Stefan
解決済! 解決策の投稿を見る。
Hi,
Yes, you understanding is correct. Thanks.
Have a great day,
Mike
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi,
Yes, you understanding is correct. Thanks.
Have a great day,
Mike
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thank you Mike!