Dear experts,
I have two questions.
1. Someone recommended to use CFG0(0x01), CFG1(0x02) as uniq ID.
(https://community.nxp.com/t5/i-MX-RT/Read-UID-Unique-ID-on-i-MXRT-RT1050/m-p/1202637)
There are 4 x 32 bits in TESTERs.
So I wonder that only 2 x 32 bits can guarantee uniq ID or not.
2.I want to lock some fields(MAC0 and/or MAC1) in OCOTP with lock register, but it can't be done.
After write MAC0 and/or MAC1, it must be protected from overwriting.
For this, MAC_ADDR field in HW_OCOTP_LOCK(0x400) must be set.
2.1 When I write MAC_ADDR field, it can't be written with below code,
OCOTP->LOCK = OCOTP->LOCK | 0x00000100;
2.2 There is error and can't be written with below code.
OCOTP_WriteFuseShadowRegister(OCOTP, 0x00, OCOTP->LOCK | 0x00000100);
I want to know how I can change Lock register in OCOTP.
Can Lock register in OCOTP only be changed with "NXP MCU Boot Utility"?
解決済! 解決策の投稿を見る。
Hi,
When you write mac address lock value, you should only write the value itself, don't write other bit again. Here you should write 0x100, not 0x40128103.
Regards,
Jing
Hi emdev,
1. I'm afraid you can't only use one 32bit register. The unique ID is not meaningless random number. Please see table 22-4 in page 776.
2. You can't write OCOTP->LOCK. It is read only register. The lock bit should be write same as other bit in ocotp.
Regards,
Jing
Dear Jingpan,
Thanks for your reply.
About answer #1, I can understand what you mean with table 22-4 in page 776.
But I can not understand answer about #2.
I can see below table in page 796.
You said OCOTP->LOCK is read only register, but above table tell me that this register is RW.
Anyway, would you let me know how I can lock OCOTP->MAC0, OCOTP->MAC1, OCOTP->GP3?
Thanks.
Hi,
But if you look into this register, you'll find almost none of its bit can be written.
You can use OCOTP_WriteFuseShadowRegister(...) to program these bits. Please note there is a mapping relationship between shadow register address and efuse address.
Regards,
Jing
Dear Jing,
I used below codes.
regAddr = 0x0;
Lock_value = OCOTP_ReadFuseShadowRegister(OCOTP, regAddr);
PRINTF("Lock value : 0x%2X : 0x%08X\n", regAddr, Lock_value);
Lock_value = Lock_value | 0x00000100;
if (kStatus_Success == OCOTP_WriteFuseShadowRegister(OCOTP, regAddr, Lock_value))
{
PRINTF("OCOTP Write operation success!\r\n");
PRINTF("The new value is 0x%08X\r\n", OCOTP_ReadFuseShadowRegister(OCOTP, regAddr));
}
else
{
PRINTF("OCOTP write operation failed. Access deny!\r\n");
}
I used register address 0x00 for LOCK and I used OCOTP_WriteFuseShadowRegister() to change register value.
But I can see "OCOTP write operation failed. Access deny!".
I checked that OCTP->CTRL value is 0x3E770200.
Would you tell me full example codes to change OCTP->LOCK?
Thanks.
Hi,
You code seems fine. What's the read back value of Lock register? The write function report fail is because CTRL[ERROR] bit is 1. This is the condition of ERROR bit become 1
If you modify the OCOTP example from writing MAC to writing MAC_ADDR lock, can it work?
Can you use MCUBootUtility to read out all fuse map?
Regards,
Jing
Dear Jing,
Below message is output from above test codes.
OCOTP controller version: 0x06000000
Lock value : 0x22 : 0x87654321
Lock value : 0x23 : 0x12345678
Lock value : 0x 0 : 0x40128003
OCOTP write operation failed. Access deny!
Lock value : 0x 0 : 0x40128003
About MCUBootUtility, I can use it.
Would you tell me what I should check with MCUBootUtility?
I'll check it.
Thanks.
Hi,
When you write mac address lock value, you should only write the value itself, don't write other bit again. Here you should write 0x100, not 0x40128103.
Regards,
Jing
Dear Jing,
With your guide, I can set Lock controls register.
Thanks.