Unable to run example on MIMXRT1170 EVKB Core M7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to run example on MIMXRT1170 EVKB Core M7

Jump to solution
492 Views
jayesh_joshi
Contributor IV

Hi 

 

I am trying to run the "mpp_camera_ultraface_view_tflm_cm7" example on the recently purchased MIMRT1170 EVKB. The results are the same for all other examples, which have "cm7" at the end.

No jumper changes on the MIMRT1170 EVKB. Image attached for reference.

 

jayesh_joshi_0-1710417792823.jpeg

 

The building and flashing steps are as below:. Is there something missing in the steps I am following? I have gone through the user guide but nothing pops out.  I am using onboard debugger for debugging. 

jayesh_joshi_1-1710417792744.png

 

 

jayesh_joshi_2-1710417792825.png

 

jayesh_joshi_3-1710417792822.png

 

 

Tags (2)
0 Kudos
Reply
1 Solution
465 Views
jayesh_joshi
Contributor IV

@EdwinHz 

Thank you for the reply.

 

Getting started guide took me to SDK of MIMXRT1170-EVK instead of MIMXRT1170-EVKB. That was the issue with example not running.

 

View solution in original post

0 Kudos
Reply
2 Replies
466 Views
jayesh_joshi
Contributor IV

@EdwinHz 

Thank you for the reply.

 

Getting started guide took me to SDK of MIMXRT1170-EVK instead of MIMXRT1170-EVKB. That was the issue with example not running.

 

0 Kudos
Reply
471 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @jayesh_joshi,

Do you see this issue with other example codes from the SDK? Or only with this one?

I noticed that MCUXpresso only imports 1 readme file, but the example seems to have 2. On the example location from the SDK installation path, you will find one readme on the main example folder and another on a subfolder called "doc".

EdwinHz_0-1710445257561.png

Here's the example location: 

"C:\Users\<user>\mcuxpresso\02\SDKPackages\SDK_2_15_000_MIMXRT1170-EVKB.zip\boards\evkbmimxrt1170\eiq_examples\mpp_camera_ultraface_view_tflm"

MCUXpresso seems to load the one under the "doc" folder, but make sure to follow both.

BR,
Edwin.

0 Kudos
Reply