USB host does not send out the PING packet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB host does not send out the PING packet

2,993 Views
iscylinfromtw
Contributor I

I'm using the USB host mode of RT1060. When I send a bulk out, I cannot see the PING packet around the DATA packet. I ensure the status of qTD token has enabled the Ping State (bit 0).

BTW, I'm not sure the PING packet is the key point to reduce the ACK time. Does someone could give me some suggestion? 

0 Kudos
Reply
4 Replies

2,955 Views
iscylinfromtw
Contributor I

You are right. If I send out the data size more than the FIFO size of USB device, USB host will start to issue a PING packet to check the receiving status.

Do you have any suggestion about how to improve the ACK time? When I tested in the Windows with same USB device, the ACK time does not over 1ms.

0 Kudos
Reply

2,933 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

But I think you should use the Time Stamp column if you want to know when ACK come back. Isn't it?

 

Regards,

Jing

0 Kudos
Reply

2,924 Views
iscylinfromtw
Contributor I

OK, Maybe I need to take a look the descriptions of the USB packet analyzer.

0 Kudos
Reply

2,980 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @iscylinfromtw ,

PING packet is not necessary during a transaction. First, USB host send a OUT packet and DATA. If the USB device return a NAK or NYET, USB host will begin to send PING. IF return ACK, it needn't to send PING.

 

Regards,

Jing

0 Kudos
Reply