Touch Input not working in custom board IMXRT 1050 using Emwin Library

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Touch Input not working in custom board IMXRT 1050 using Emwin Library

951 Views
yvkrkrishna
Contributor III

Hi,

I am using IMX RT 1050 micro controller EVK Board along with LCD size 480x272.

I have made my own custom GUI using appwizard and integrated into MCU Expresso IDE.

I have flashed the GUI into LCD and touch input is working properly using following emwin_support.c configuration parameters:

// LCD Size 480x272 EVK Board
#define APP_IMG_HEIGHT 272
#define APP_IMG_WIDTH 480
#define APP_HSW 41
#define APP_HFP 4
#define APP_HBP 8
#define APP_VSW 10
#define APP_VFP 4
#define APP_VBP 2

#define LCD_WIDTH 480
#define LCD_HEIGHT 272
#define LCD_BITS_PER_PIXEL 32

Now i am using custom board with LCD size 800x480 (Make AZ Systems) resolution using the same touch IC: FT 5336.

I have made GUI of size 800x472 using app wizard software and able to flash successfully into LCD.

But problem is:

Touch input is working only in first quadrant of LCD Display. I have used the following emwin_Support.c parameters: as per datasheet

#define APP_IMG_WIDTH 800//800
#define APP_IMG_HEIGHT 480//480
#define APP_HSW 48
#define APP_HFP 40
#define APP_HBP 40
#define APP_VSW 3
#define APP_VFP 13
#define APP_VBP 29

#define LCD_WIDTH 800//800//480
#define LCD_HEIGHT 480//480//272
#define LCD_BITS_PER_PIXEL 32//32

 

Is there any other configuration  to be changed??

Could anyone guide me how to resolve the touch input issue mentioned above ASAP.

I have attached the Data Sheets of custom LCD & EVK LCD, Emwin_support.c files.

 

Thanks & Regards

Krishna Reddy

Mob: 9620620953

Labels (1)
0 Kudos
Reply
0 Replies