Hi,
About address 402B_8004 ~ 402B_800C (LCDIF_CTRL_SET, CLR, TOG) in IMXRT1064RM_reference_manual,
I can not see register description for them, just for 402B_8000 (LCDIF_CTRLn)
Where can I find these register descriptions?
Thanks & best regards
已解决! 转到解答。
Hi @anthonyama ,
You mean these register, right:
From my experience, the SET register means, when you write the related bit to 1, the related bit will be SET, CLR is when you write the related register to 1, the related bit will be clear, ToG is will toggle the related bit.
In fact, the RM is also mentioned it:
I suggest you use the CTRL, CTRL1, CTRL2 register write directly instead of the SET, CLR, TOG register, that will be more easy to understand in the RM.
Wish it helps you!
Best Regards,
Kerry
Hi @anthonyama ,
You mean these register, right:
From my experience, the SET register means, when you write the related bit to 1, the related bit will be SET, CLR is when you write the related register to 1, the related bit will be clear, ToG is will toggle the related bit.
In fact, the RM is also mentioned it:
I suggest you use the CTRL, CTRL1, CTRL2 register write directly instead of the SET, CLR, TOG register, that will be more easy to understand in the RM.
Wish it helps you!
Best Regards,
Kerry