Speed of CAN3 module in FlexCan SDK example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Speed of CAN3 module in FlexCan SDK example

Jump to solution
480 Views
Jeevan
Contributor IV

Hi team,

We are using CAN3 module in imxrt1176 controller.

To test the CAN operation we are connect CAN_HI, CAN_LO, GND of one board to another board respectively and used the FlexCan SDK example and the single byte of Data is transfered between the 2 boards.

What is the speed of CAN used in this example code for imxrt1176 controller using FlexCan

Tags (2)
0 Kudos
Reply
1 Solution
422 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @Jeevan 
You can check the default configuration of the FlexCan in a comment on any SDK example for FlexCAN, for example flexcan_interrupt:

Pablo_Ramos_0-1714685739109.png

 

View solution in original post

0 Kudos
Reply
1 Reply
423 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @Jeevan 
You can check the default configuration of the FlexCan in a comment on any SDK example for FlexCAN, for example flexcan_interrupt:

Pablo_Ramos_0-1714685739109.png

 

0 Kudos
Reply