Speed of CAN3 module in FlexCan SDK example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Speed of CAN3 module in FlexCan SDK example

跳至解决方案
991 次查看
Jeevan
Contributor IV

Hi team,

We are using CAN3 module in imxrt1176 controller.

To test the CAN operation we are connect CAN_HI, CAN_LO, GND of one board to another board respectively and used the FlexCan SDK example and the single byte of Data is transfered between the 2 boards.

What is the speed of CAN used in this example code for imxrt1176 controller using FlexCan

标记 (2)
0 项奖励
回复
1 解答
933 次查看
Pablo_Ramos
NXP Employee
NXP Employee

Hi @Jeevan 
You can check the default configuration of the FlexCan in a comment on any SDK example for FlexCAN, for example flexcan_interrupt:

Pablo_Ramos_0-1714685739109.png

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
934 次查看
Pablo_Ramos
NXP Employee
NXP Employee

Hi @Jeevan 
You can check the default configuration of the FlexCan in a comment on any SDK example for FlexCAN, for example flexcan_interrupt:

Pablo_Ramos_0-1714685739109.png

 

0 项奖励
回复