Regarding the core clock of the i.MX RT595

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Regarding the core clock of the i.MX RT595

559 次查看
adc_6_6
Contributor II

Hello.

Could you please tell me if it's possible to change the core clock while operating on RT595?

For example, increasing the clock before performing a high-load process and then lowering it afterwards.

Thank you.

0 项奖励
回复
4 回复数

473 次查看
adc_6_6
Contributor II

@Omar_Anguiano

thank you for your reply.

I understand the rules.

In this case, is there a regulation regarding the interval between changing the clock and adjusting the voltage?
Additionally, how long does it take for the system to stabilize after making these changes?

Best regards

0 项奖励
回复

433 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Yes, you can see the voltage and its maximum frequency on the datasheet under the general operating conditions chapter.
For the main system it is characterized a maximum of 150us but this value may vary.

Best regards,
Omar

0 项奖励
回复

395 次查看
adc_6_6
Contributor II

@Omar_Anguiano 

Hello

Thank you for your reply.
I will check it.

Best regards,
adc_6_6

0 项奖励
回复

526 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

You need to set an alternate clock to be used as main clock while you change the frequency of your clock. 
When the frequency of Core needs to change the voltage of the Core also need to be change. There is a rule in changing core frequency and voltage.
• Increasing core frequency, voltage first, then frequency.
• Decreasing core frequency, frequency first, then voltage.

Best regards,
Omar

0 项奖励
回复