RT1176 MU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1176 MU

270件の閲覧回数
Zhang_123
Contributor II

I transplanted the MU function and tested the time from sending to receiving using single channel test 164ms,it‘s  too slow

Do we have ways to improve efficiency?

0 件の賞賛
1 返信

235件の閲覧回数
PabloAvalos
NXP TechSupport
NXP TechSupport

Dear @Zhang_123 

 

Thanks a lot for reaching our technical support on our community. I really appreciate your patience here.

 

Regarding a way to improve efficiency on MU example, there is no way to do it, due to the performance-wise, using the MU is that kind of slow since it is sending byte per byte through the Messaging Unit interface to the another core, so probably RPMSG-lite can be a copy-less communication mechanism, making it very fast and it can also send as many bytes as needed in a single message.

 

Hope this information can help you, please let me know if you have more questions.

 

BR.
Pablo Avalos.

0 件の賞賛