I'm designing a board with i.MX RT1170.
I plan to use MCU Link debug probe for debugging, so I'm preparing 10-pin connector on my board.
I have some question about the pin connection on the board.
Question
1. Regarding Pin10, which should I connect JTAG_nTRST(GPIO_LPSR_10) or POR_B?
2. Regarding Pin6, is it enough to connect only JTAG_MUX_TDO(GPIO_LPSR_11)?
Could you share if there is a reference design how to implement 10-pin SWD connector on a board with RT1170.
已解决! 转到解答。
1. Connect it to GPIO_LPSR_10, if connected to POR_B you will need to ensure that POR_B remains asserted during the whole power-up sequence.
2. Yes, you can add pulls but they are not needed. For connection recommendations, I suggest you refer to the hardware development guide as well as the EVK schematic.
Best regards,
Omar
1. Connect it to GPIO_LPSR_10, if connected to POR_B you will need to ensure that POR_B remains asserted during the whole power-up sequence.
2. Yes, you can add pulls but they are not needed. For connection recommendations, I suggest you refer to the hardware development guide as well as the EVK schematic.
Best regards,
Omar