RT1170 flexSPI XiP max serial clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1170 flexSPI XiP max serial clock

797 Views
nickwallis
Senior Contributor I

Hi,

I want to check, please can you tell me all the settings we need to change to make the SDK projects run at maximum QSPI serial clock frequency for XiP applications?

We already made sure to float the DQS pin in our schematics (GPIO_SD_B2_05).

We also made sure in evkmimxrt1060_flexspi_nor_config.c that readSampleClkSrc is set to kFlexSPIReadSampleClk_LoopbackFromDqsPad;

What other settings are needed to ensure max speed operation from external QSPI flash (133 MHz)?

Our external QSPI flash is MX25U12832FM2I02.

many thanks!

0 Kudos
Reply
3 Replies

768 Views
nickwallis
Senior Contributor I

@jingpan thanks, but I meant from a software point of view (apologies this wasn't clear).

In the SDK, which setting(s) have to be changed in which source module(s) to ensure maximum QSPI serial clock frequency operation?

thanks!

0 Kudos
Reply

762 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @nickwallis ,

What you have done is enough. Next step, just configure the input clock to 133Mhz.

jingpan_0-1675997713702.png

 

Or if you didn't change the qspflash_config, serialClkFreq is kFlexSpiSerialClk_133MHz already. That means ROM boot will set the flexspi frequency to 133Mhz before jump to your application. So, you needn't do anything.

Regards,

Jing

 

0 Kudos
Reply

775 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @nickwallis ,

That's fine. Please also refer to hardware design guide about flexspi layout recommendation.

 

Regards,

Jing

0 Kudos
Reply