RT1170 GPIO Operating Range setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1170 GPIO Operating Range setting

ソリューションへジャンプ
776件の閲覧回数
Eugene3
Contributor II

How can I set 3.3V mode or 1.8V mode for GPIO_SD?

GPIO_LPSR, AD and DISP have register for supply voltage range selection. But I couldn't find similar register for GPIO_SD and EMC.

Is the mode simply selected by the NVCC_XX power rail voltage without register setting?

0 件の賞賛
1 解決策
722件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @Eugene3 ,

The pad work in 3.3v mode or 1.8v mode is designed by hardware. NVCC_SD is the power source of SD pin group. You can refer to RT1170 EVK schematic for how to switch.

jingpan_0-1694670727224.png

 

Regards,

Jing

 

元の投稿で解決策を見る

0 件の賞賛
4 返答(返信)
723件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @Eugene3 ,

The pad work in 3.3v mode or 1.8v mode is designed by hardware. NVCC_SD is the power source of SD pin group. You can refer to RT1170 EVK schematic for how to switch.

jingpan_0-1694670727224.png

 

Regards,

Jing

 

0 件の賞賛
716件の閲覧回数
Eugene3
Contributor II

Hi @jingpan 

Can I also apply same way to other power rails to set 1.8V/3.3V mode?

ex. If I use 1.8V power to NVCC_EMC1, will GPIO_EMC_B1_XX work in 1.8V range?

0 件の賞賛
665件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @Eugene3 ,

Yes, it can.

 

Regards,

Jing

0 件の賞賛
624件の閲覧回数
Eugene3
Contributor II

Thank you.

I understand.

0 件の賞賛