RT1064 RT1050 ADC VDDA_ADC_3P3 Supply Current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1064 RT1050 ADC VDDA_ADC_3P3 Supply Current

516 Views
andyhewitson
Contributor I

Hi,

Working on a new RT1064 design.  Since Vrefh is bonded to VDDA_ADC_3P3, I'd like to drive VDDA_ADC_3P3 with a reference, instead of using the [relatively] noisy 3.3V supply.

I'm struggling to find a supply requirement for VDDA_ADC_3P3.  Page 23 of IMXRT1064CEC says that max is 40mA.  If I'm reading it correctly, 33mA of that is for the resistive touch screen (worst case).  I'm not using the Touch Screen Controller.  Does that mean that without the TSC, VDDA_ADC_3P3 max is 7mA for both converters running at 1MS/s?  Seems a bit light.

TIA, Andy.

Labels (2)
0 Kudos
Reply
1 Reply

471 Views
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

Running at running at 1MS/s is not specified. However, you can find more details of typical values and conditions in Table 55. 12-bit ADC characteristics (VREFH = VDDA, VREFL = VSSAD) of the datasheet.

Hope it helps you.

Have a nice day!

0 Kudos
Reply