Hi,
we are a bit confused from other threads and documentation about the BOOT_MODE and BT_CFG pins / fuses with the RT1062.
We are working on a custom board based on the RT1062.
For manufacturing what we want to achieve is:
The board comes in serial downloader, downloads its initial application to flash and then we burn fuses in order to always boot from the flash.
Do I understand Gary Segal in this thread correctly that we can leave all BOOT_MODE and BT_CFG pins floating to achieve that? Is this also valid for the RT1062?
How specifically should we set / connect BOOT_MODE and BT_CFG to achieve what we plan on doing?
(Boot to Serial Downloader initially -> Download binary & burn fuses from there -> Boot from fuses (Flash))
Looking forward to you answer!
Thanks!
Paul
Hi Paul Brandt ,
I don't recommend you let the BOOT_CFG and BOOT_MODE as float, it is not stable.
You can check the following boot mode in the RT RM, it is useful to you:
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------