RT1060 - HDMI output solution w/ 8-bit LCD bus?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1060 - HDMI output solution w/ 8-bit LCD bus?

Jump to solution
1,611 Views
dmarks_ls
Senior Contributor I

So I'm creating a new RT1060-based design, and I want to provide two Ethernet ports.  We're using SDRAM, so the entire GPIO_EMC bank is unavailable.  This means that for ENET 2 I have to use GPIO_B0_12 through GPIO_B1_03 (if I don't want to overlap USDHC1 on GPIO_SD_B0_00-05).  Unfortunately, that takes away LCD_DATA[8-15] and leaves only LCD_DATA[7-0] and the four control signals, which is annoying because that appears to complicate connecting the LCDIF to an HDMI transmitter IC.

I know it's possible to get the LCDIF to drive an 8-bit bus with 24-bit pixel data; that's illustrated in Figure 35-4 in the reference manual, where it kicks out bytes B, C, and D on three separate clocks.  Unfortunately, I can't seem to find an HDMI/TMDS transmitter that would accept such a bus interface.

  • The Analog Devices ADV7513 seems to be a close match, but according to the programming guide it will only accept 2 clocks worth of pixel data (not 3), and it only accepts RGB data in a single-clock fashion.  (Same for the ADV7511W and its programming guide.)
  • The Texas Instruments TFP410 would also seem to be a candidate, but it accepts only a 12-bit or 24-bit input bus, no option for 8-bit.  And the 12-bit mode is DDR (latches on both rising and falling edge).
  • There's an NXP TDA19988 part out there, but there's very little info available about it; here's a Digi-Key link, and here's a forum thread link.  Unfortunately, it only appears to offer 12-bit or 24-bit bus input, not 8-bit.

Is anyone aware of a solution that will take an 8-bit TTL/CMOS input and generate an HDMI/DVI/DisplayPort output?  I realize that I could probably use any of the above chips if I just put a little FPGA between the RT1060's 8-bit LCD bus and the 24-bit HDMI transmitter input bus, and have the FPGA accept three clocks' worth of data before clocking all 24 bits out to the HDMI chip.  Just wondering if there's a single-chip solution for this.  Thanks.

David R.

Tags (3)
0 Kudos
Reply
1 Solution
1,558 Views
jeremyzhou
NXP Employee
NXP Employee

Hi David Rodgers,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
According to your statement, I think the FPGA is essential to your solution.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,559 Views
jeremyzhou
NXP Employee
NXP Employee

Hi David Rodgers,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
According to your statement, I think the FPGA is essential to your solution.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,558 Views
dmarks_ls
Senior Contributor I

Hi Jeremy,

That's kinda what I figured; if a customer really needs SD card + two Ethernet + HDMI out, then we can spin them a board with an extra little FPGA/CPLD on it.  Thanks.

David R.

0 Kudos
Reply