RT1052 LPUART FIFO depth is only 1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1052 LPUART FIFO depth is only 1?

2,404 Views
lixiaotian
Contributor I

the LPUART Parameter Register (PARAM) is read as 0. So what is the meaning of the fifo?

Labels (1)
0 Kudos
Reply
5 Replies

2,117 Views
1277185193
Contributor III

?????????????????????????????????????????????????????????????????????

0 Kudos
Reply

2,117 Views
jeremyzhou
NXP Employee
NXP Employee

Hi li xiaotian,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Please check the LPUART[FIFO] register.

pastedImage_1.png


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,117 Views
1277185193
Contributor III

Excuse me ...How to change the fifo depth? This field is read only......B8JKEAKPH0~9X6(7E_{784D.png

0 Kudos
Reply

2,117 Views
jeremyzhou
NXP Employee
NXP Employee

Hi 卢 鲲,

Thanks for your reply.
It's not able to customize to configure the depth of the buffer, you only can enable the buffer or discard this feature.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,117 Views
1277185193
Contributor III
  • OK!  Excuse me ......Are you an official with NXP ?

    It's so unbelievable...Why are there so many options of fifosize?
0 Kudos
Reply