[RT1050] Start wlan download fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[RT1050] Start wlan download fail

Jump to solution
1,394 Views
yen_chen
Contributor III

Hi,all

when I download wlan fw it will stop in SDMMCHOST_TransferFunction.

why the event can not response ?

normal process will run FW ready and wlan fw download successful

0125.png

Have anything I forget setting?

0 Kudos
Reply
1 Solution
1,370 Views
yen_chen
Contributor III

Hi @kerryzhou 

I solve this problem

I revised some setting .

setting->MCU Linker -> Managed Linker Script

0126_1.png

Thank you for your support~

Br,

Yen

View solution in original post

7 Replies
1,372 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi yen_chen,

  I checked :\SDK_2.9.0_EVKB-IMXRT1050\boards\evkbimxrt1050\wifi_examples\wifi_cli

  This project requirement:

Hardware requirements
=====================
- Micro USB cable
- evkbimxrt1050 board
- Personal Computer
- One of the following WiFi modules:
- Panasonic PAN9026 SDIO ADAPTER + SD to uSD adapter
- AzureWave AW-NM191NF-uSD
- AzureWave AW-AM457-uSD

If you want use the AzureWave AW-NM191NF-uSD, please change the project macro WIFI_BOARD_PAN9026_SDIO to WIFI_BOARD_AW_NM191.

This is my AzureWave AW-NM191NF-uSD, do you use the same board? Please check your board hardware.

image.png

I am using the AzureWave AW-NM191NF-uSD and test:

SDK_2.9.0_EVKB-IMXRT1050\boards\evkbimxrt1050\wifi_examples\wifi_cli

Will give you the test log later.

 

Best Regards,

Kerry

 

0 Kudos
Reply
52 Views
James12
Contributor II
Hi kerryzhou. Could you tell me where I can get AW-NM191NF-uSD? Thank you.
0 Kudos
Reply
1,391 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi yen_chen

  Do you use the NXP official SDK code on your side?

  If yes, please tell me which SDK version, which detail code you are using? You are using wifi, please also tell me which WIFI module you are using now.

  Do you use the MIMXRT1050-EVKB board?

 Please also let me know your testing IDE.

  Then I can help you to check more details.

Best Regards,

Kerry

0 Kudos
Reply
1,389 Views
yen_chen
Contributor III

Hi @kerryzhou 

I use SDK_2.8.6, EVKB-IMXRT1050-OM13588

WIFI Board : WIFI_BOARD_AW_NM191MA

I use wifi_example : wifi_cli to port my project but can not download FW.

 

0 Kudos
Reply
1,377 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Thanks for your updated information!

Your SDK version is a little old, you can use this SDK_2.9.0_EVKB-IMXRT1050 this version, which can be downloaded from this link:

https://mcuxpresso.nxp.com/

I will test it today with the newest SDK2.9.0, and give you reply later, please keep patient!

 

Best Regards,

Kerry

0 Kudos
Reply
1,371 Views
yen_chen
Contributor III

Hi @kerryzhou 

I solve this problem

I revised some setting .

setting->MCU Linker -> Managed Linker Script

0126_1.png

Thank you for your support~

Br,

Yen

1,361 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Thanks for your solution sharing.

 The SDK related code project also have this configuration.

 If you have any question in the future, welcome to create the new question post.

Best Regards,

Kerry