RT1050 EVKB QSPI Flash XIP Failed (AN12183)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1050 EVKB QSPI Flash XIP Failed (AN12183)

ソリューションへジャンプ
2,798件の閲覧回数
yi-yuanting
Contributor III

Hi,

I have both EVKA and EVKB of rt1050.

Our rt1050-based product need to use QSPI flash instead of hyper flash, so we are studying it.

I have followed all step of doc: AN12183, but I got different results below.

[EVKA: QSPI XIP Succeed]

According to AN12183,

(1) I removed the hyper flash and welded 0 ohm resistor from R153 to R158

(2) I updated FW of CMSIS-DAP (for QSPI NOR Flash).

(3) I changed flash setting code according to AN12183SW.zip and use IAR to run debug in XIP mode

The result is successful. System runs in XIP mode.

EVKA_Success.png

But when I used EVKB, I got failed result!!

[EVKB: QSPI XIP Failed]

According to AN12183,

(1) I don't need to remove hyper flash. I removed R356,R361~R366 and welded 0 ohm from R153 to R158.

(2) I updated FW of CMSIS-DAP (for QSPI NOR Flash).

(3) I changed flash setting code according to AN12183SW.zip and use IAR to run debug in XIP mode

The result is failed......

(4) SDK version: 2.4.0

EVKB_Fail2.png

We all knew that rt1050-A0 and EVKA were deprecated, so we need your help to solve the QSPI problem in EVKB ! Thanks!

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
1,808件の閲覧回数
yi-yuanting
Contributor III

Hi igor,

We solved this issue 5mins ago.

I must apologize first, the reason is that our hardware engineer add two 0 ohm resister R358 and R359, which are incorrect, so QSPI flash can't run.

After remove R358 and R359, system can run on QSPI now.

Thank you.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,808件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yi-Yuan

please check differencies between EVKA and EVKB boards and software used for them

i.mx rt1050 DR_SET and DR_CLEAR 

Useful information for RT1050 

How to i.MXRT1051 QSPI Boot w/o XIP (Reside in Flash, Run from TCM) 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,809件の閲覧回数
yi-yuanting
Contributor III

Hi igor,

We solved this issue 5mins ago.

I must apologize first, the reason is that our hardware engineer add two 0 ohm resister R358 and R359, which are incorrect, so QSPI flash can't run.

After remove R358 and R359, system can run on QSPI now.

Thank you.

0 件の賞賛
返信
1,808件の閲覧回数
gideonintrater
Contributor I

Hi Yi-Yuan, have you considered lower-cost Octal devices rather than switching to a Quad and reducing your XiP performance?

0 件の賞賛
返信