Hi,
I have both EVKA and EVKB of rt1050.
Our rt1050-based product need to use QSPI flash instead of hyper flash, so we are studying it.
I have followed all step of doc: AN12183, but I got different results below.
[EVKA: QSPI XIP Succeed]
According to AN12183,
(1) I removed the hyper flash and welded 0 ohm resistor from R153 to R158
(2) I updated FW of CMSIS-DAP (for QSPI NOR Flash).
(3) I changed flash setting code according to AN12183SW.zip and use IAR to run debug in XIP mode
The result is successful. System runs in XIP mode.
But when I used EVKB, I got failed result!!
[EVKB: QSPI XIP Failed]
According to AN12183,
(1) I don't need to remove hyper flash. I removed R356,R361~R366 and welded 0 ohm from R153 to R158.
(2) I updated FW of CMSIS-DAP (for QSPI NOR Flash).
(3) I changed flash setting code according to AN12183SW.zip and use IAR to run debug in XIP mode
The result is failed......
(4) SDK version: 2.4.0
We all knew that rt1050-A0 and EVKA were deprecated, so we need your help to solve the QSPI problem in EVKB ! Thanks!
解決済! 解決策の投稿を見る。
Hi igor,
We solved this issue 5mins ago.
I must apologize first, the reason is that our hardware engineer add two 0 ohm resister R358 and R359, which are incorrect, so QSPI flash can't run.
After remove R358 and R359, system can run on QSPI now.
Thank you.
Hi Yi-Yuan
please check differencies between EVKA and EVKB boards and software used for them
i.mx rt1050 DR_SET and DR_CLEAR
How to i.MXRT1051 QSPI Boot w/o XIP (Reside in Flash, Run from TCM)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
We solved this issue 5mins ago.
I must apologize first, the reason is that our hardware engineer add two 0 ohm resister R358 and R359, which are incorrect, so QSPI flash can't run.
After remove R358 and R359, system can run on QSPI now.
Thank you.
Hi Yi-Yuan, have you considered lower-cost Octal devices rather than switching to a Quad and reducing your XiP performance?