How do you put RT1170-EVK into "ISP USB mode" in order to update MCU-Link firmware?
My goal was to compare JLINK versus CMSIS-DAP debugger functionality under MCUXpresso.
Thanks in advance,
-Ed
MCU-Link update to JLINK
Solved! Go to Solution.
@jingpanI I understand now. Thank you for the solution.
The following links and app notes apply to both the RT10xx and RT1170 EVK boards, except '''J22''' is the RT1170-EVK equivalent DFU (Device Firmware Upgrade) jumper to '''J42''' on RT1060-EVK.
U24 chip found on the RT1170 EVK board is a LPC4322 microcontroller implementing the debug probe and can be programmed using LPCScrypt v2.1.2
I now have my RT 1170 EVK detecting as a JLINK debugger under MCUXpresso.
Thank you for your patience and assistance.
-Ed
Hi @EdOfTheMountain ,
Please refer to AN13206.
https://www.nxp.com/docs/en/application-note/AN13206.pdf
Regards,
Jing
H Jing,
The app note is for the i.MX RT10xx boards.
I am using the i.MX RT1170 EVK board.
Can you please help me with the MIMXRT1070-EVK ?
The AN13206 app note refers to J42 on MIMXRT1060-EVK, to force DFU boot mode. The MIMXRT1070-EVK does not have a J42?
Can MCU-Link installer for Windows 10 be used with MIMXRT1070-EVK ?
https://www.nxp.com/design/microcontrollers-developer-resources/mcu-link-debug-probe:MCU-LINK#t996
Thank you,
-Ed
Hi @EdOfTheMountain ,
I think they are same. The jumper on RT1170-EVK is J22.
Can MCU-Link installer for Windows 10 be used with MIMXRT1070-EVK ?
Yes.
Regards,
Jing
Hi @jingpan
RT1170-EVK J22 did not work for me?
Can you please help determine what I am doing wrong?
What I have tried:
1) I downloaded and installed MCU-Link installer for Windows 10
2) Power-off RT 1170 EVK, disconnect USB cable from Windows Host (J11 on EVK board)
3) Run Program MCU-LINK JLINK, and the program displays:
Place the board in ISP USB mode using the appropriate jumper on your MCU-Link.
Refer to the board documentation for more information.
Connect board via USB then press Space.
Press any key to continue . . .
4) I installed bridge jumper on RT 1170 EVK board J22 as you suggested.
5) Connect USB cable to Windows Host (J11 on EVK board)
6) Press space to continue,
7) Program continues to prompt "Configure board for ISP mode and connect via USB then press Space.
Press any key to continue . . ."
See screenshot below:
See picture of my EVK board MIMXRT1170-EVK
Where can find documentation for EVK jumpers and "ISP Mode" found for RT 1170 EVK?
Thank you for your help
-Ed
Hi @EdOfTheMountain ,
You used wrong tool. MCUlink is LPC55S69 core. You should use LPCScrypt. Please read that application notes.
Regards,
Jing
@jingpanI I understand now. Thank you for the solution.
The following links and app notes apply to both the RT10xx and RT1170 EVK boards, except '''J22''' is the RT1170-EVK equivalent DFU (Device Firmware Upgrade) jumper to '''J42''' on RT1060-EVK.
U24 chip found on the RT1170 EVK board is a LPC4322 microcontroller implementing the debug probe and can be programmed using LPCScrypt v2.1.2
I now have my RT 1170 EVK detecting as a JLINK debugger under MCUXpresso.
Thank you for your patience and assistance.
-Ed
I wanted to put a clarifying note about the i.MX RT1170 EVKs here.
There are two different eval boards for this processor with different order numbers, and they have different debug probes. Both can run a CMSIS-DAP based image from NXP or an evaluation version of J-Link from SEGGER: