Hi all.
I want to use a 24M oscillator(3.3V) to connect to XTALO. But the logic level of this forcing clock must not exceed the NVCC_PLL level(Typical Programming Operating Range is 1.0V to 1.2 V with the nominal default setting as 1.1 V).
My question is whether i can use two resistances to divide the output of oscillator to satisfy the requirement of XTALO DC parameters.And the precision of NVCC_PLL.
Hi,
This has not been tested but it looks like it could work. Please just take into considerations that 'the crystal must be rated for a maximum drive level of 250 uW as it is stated in datasheet.
Best regards,
Felipe