Not able to Flash on i.MRT1176 .Failed on connect: Ee(42). Could not connect to core. No connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to Flash on i.MRT1176 .Failed on connect: Ee(42). Could not connect to core. No connection

1,785 Views
Ankarao_Ittadi
Contributor I

Hi

When we are debugging RT1176, we are facing followinng issue.

Any body Please help us.

Tags (1)
0 Kudos
Reply
3 Replies

1,779 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To be prudent, I'd like to know what exactly board you used.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,778 Views
Ankarao_Ittadi
Contributor I

Hi we are Using Embedded  Artists i.MX RT1176 Developers kit (Rev PB2) Board.

 

You can find the more details on this link also.

 

https://www.embeddedartists.com/products/imx-rt1176-ucom/

#i.MX RT1176 EA(Embedded Artists)

0 Kudos
Reply

1,771 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @Ankarao_Ittadi ,
Thanks for your reply.
Maybe you can try the below trick to recover.
1) Set the boot mode pins to Serial Downloader.
2) Power on the board, debug the demo project.
3) After that, power off and recover the boot mode pins to the previous set, then power on again.
4) Give a debug again.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply