MAX17260 Battery Connection or Removal Status in IMXRT 1050 controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MAX17260 Battery Connection or Removal Status in IMXRT 1050 controller

594 次查看
yvkrkrishna
Contributor III

Hi,

I am using IMXRT 1050 micro controller and MAX 17260 chip for battery capacity reading.

Now i want to check whether battery is connected or removed.

As per the datasheet i am reading the register "CONFIG REGISTER" it is always coming value as 0x2210

In CONFIG Register(0x1D),

Bit positions:

0th bit  D0 - Ber     (battery Removal)

1st bit  D1 - Bei     (battery Insertion)

Can anyone please guide me how to get the connection or removal status of MAX 17260 battery.

标签 (1)
0 项奖励
回复
1 回复

584 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I think you'd better contact Maxim integrated apply for some advice or suggestions, as I'm not familiar with their products.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------