Hi,
I am using 100-pin MIMXRT1021CAF4A and want to interface Ethernet PHY chip.
I see that ENET_MDIO & ENET_MDC pins are shared with JTAG pins.
In 144-pin package these pins are dedicated.
Evaluation kit schematic uses 144-pin package.
I just want to confirm that I have to share these two pins with JTAG ?
Thanks
Suhas
Hi Suhas,
Yes, you have to share the pin. If you don't want share, you can use SWD debug instead of JTAG. GPIO_AD_B0_04 and GPIO_AD_B0_05 is not used by SWD.
Regards,
Jing