Internal flash on RT 1064 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Internal flash on RT 1064 ?

跳至解决方案
2,586 次查看
carstengroen
Senior Contributor II

I have the EVK 1064 which runs just fine. I'm in the process of designing my first board with the RT 1064, and in that process I have a hard time finding info on the internal (QSPI?) Flash. On the EVK, I have the Flash at 0x70000000 and according to the UM this is FlexSPI2 interface. Is that connected to the internal flash of the CPU, or is this the external flash (on the EVK) ?

What pins on the CPU is used (I assume that some of the pins are connected both to external pins as well as the internal Flash chip) ?

I have not (yet) been able to find info on the internal flash in the manuals so far...

1 解答
1,984 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Carsten

info on the internal flash can be found in

AN12290 Migration Guide from i.MX RT1060 to i.MX RT1064

https://www.nxp.com/docs/en/application-note/AN12290.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
1,984 次查看
jay_heng
NXP Employee
NXP Employee
0 项奖励
回复
1,985 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Carsten

info on the internal flash can be found in

AN12290 Migration Guide from i.MX RT1060 to i.MX RT1064

https://www.nxp.com/docs/en/application-note/AN12290.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,984 次查看
carstengroen
Senior Contributor II

Thanks a lot Igor!

I don't quite know how that document slipped my eyes in the first place :smileyhappy:

Thanks!

0 项奖励
回复