Interface with AD9364

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interface with AD9364

999 Views
Anburaja
Contributor I

Hi,

I want to configure and control the AD9364 with i.MX RT1170 controller ,if it is possible?

0 Kudos
Reply
5 Replies

991 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Anburaja ,

   In fact, whether the AD9364 is supported, just check your used chip interface, I check it, find it contains the SPI, and parallel interface.

  So, RT1170 can support it, as it contains the LPSPI and the flexIO support the parrallel, even the normal GPIO also can use as the parallel input and output.

Best Regards,

kerry

 

0 Kudos
Reply

986 Views
Anburaja
Contributor I

Thanks for your reply Kerry,

You suggested [RT1170], it works up to 1 GHz, but I need to use up to 3 GHz, any other IC?

0 Kudos
Reply

976 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Anburaja ,

  To the MCU, no 3GHz, the highest is 1Ghz.

   If you need higher speed, you may need to check the MPU, not the MCU.

 BTW, do you mean your chip spi and the parallel IO is up to 3Ghz, I don't think that is possible.

   Maybe you need to double check your requirement at first.

 

Best Regards,

Kerry

0 Kudos
Reply

956 Views
Anburaja
Contributor I

ok fine.

Is there any other way to make the MCU or MPU work up to 3GHz? Send if suitable IC available.

 

Thanking you..!

0 Kudos
Reply

951 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Anburaja ,

  At least our RT have no way to run upto 3G, as you know, the core is just upto 1G.

  To the MPU, you may check it in this area, you can create a new question about MPU :

https://community.nxp.com/t5/i-MX-Processors/bd-p/imx-processors

Not the RT, then our MPU engineer will help you.

 

Wish it helps you!

Best Regards,

kerry

0 Kudos
Reply