Implement Echo Canceller on MIMXRT685-AUD-EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Implement Echo Canceller on MIMXRT685-AUD-EVK

768件の閲覧回数
AS3
Contributor I

Hi,
I would like to implement acoustic echo-canceller on the MIMXRT685-AUD-EVK. To this end, I would need a reference signal which is the signal played in the speaker. But, this reference signal should be synched with the signals captured by the microphones. 
Usually, there is a HW loopback either from the output of the CODEC back through A2D, or from the I2S output to a different I2S input.
Can you recommend how do I configure such HW loopback? 
Thanks, A. 

0 件の賞賛
返信
2 返答(返信)

731件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me check the following post ?

 

https://community.nxp.com/t5/i-MX-RT/Noise-and-Echo-cancellation-application-with-MIMXRT685/m-p/1283...

 

Regards

0 件の賞賛
返信

723件の閲覧回数
AS3
Contributor I

Hello @estephania_mart ,
I know this post (I scanned the forum for echo cancellation), but it is not valuable to my questions.

Sorry, and hope to get a more concrete answer.
Thanks, AS3

0 件の賞賛
返信