IMXRT1064 MCUXpresso SPT - Flash Programmer Tool - Recovery - EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1064 MCUXpresso SPT - Flash Programmer Tool - Recovery - EVK

Jump to solution
648 Views
Lukas_Frank
Senior Contributor I

Hi Dear Authorized,

 

I apply the recovery procedure to my EVK seen in Figure Set 1. Because I got below error. After apply recovery procedure I think that this error will be disappear. But it still continue. However, I tried to debug my EVK with different workspace it works correctly. I can't understand the issue. Why I can't debug my EVK with the workspace which I was able to debug successfully before. Do you have any idea?

 

Thanks and Regards. 

 

Lukas_Frank_0-1692590193503.png

 

 

 

Figure Set 1 : Applied Recovery Procedure with MCUXpresso SPT

Lukas_Frank_1-1692590380256.pngLukas_Frank_2-1692590389407.pngLukas_Frank_3-1692590415452.png

Lukas_Frank_4-1692590773781.pngLukas_Frank_5-1692590798468.pngLukas_Frank_6-1692590806743.png

Lukas_Frank_7-1692590814416.png

 

 

Labels (1)
0 Kudos
Reply
1 Solution
577 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, sorry for the late response, the curious behaviors were new for me, and then I noticed this.

    It seems that using a 1024 project on RT1064, which will cause a wrong, which means FCB, to be downloaded. Please help confirm that, and using the same project with the board:

Pavel_Hernandez_0-1692920122983.png

Best regards,
Pavel

View solution in original post

4 Replies
578 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, sorry for the late response, the curious behaviors were new for me, and then I noticed this.

    It seems that using a 1024 project on RT1064, which will cause a wrong, which means FCB, to be downloaded. Please help confirm that, and using the same project with the board:

Pavel_Hernandez_0-1692920122983.png

Best regards,
Pavel

547 Views
Lukas_Frank
Senior Contributor I

Hi Dear @Pavel_Hernandez ,

 

I tried too many combinations. After a while, I pass some steps spontaneusly. 

 

Thank you soo much for your helps.

0 Kudos
Reply
620 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, let me get into your case and when I have more information, I will contact you.

Best regards,
Pavel

0 Kudos
Reply
606 Views
Lukas_Frank
Senior Contributor I

Hi Dear @Pavel_Hernandez ,

 

Thank you so much.

0 Kudos
Reply