hi @kerryzhou
thanks for your help, i realized the problem... i was using the wrong JTAG header J29 instead of J16.
Hi @Irv95G ,
Do you mean, you are using the external LPC-LINK2 in stead of the on board CMSIS DAP debugger?
If you are using the external debugger, you need to disconnect the on board debugger, J47-J50.
Then connect your external LPC-LINK2 to the j16 jtag port, in your MCUXpresso, please also press shift+debug button, to recognize the external debugger again. Or you can delete the .launch file, then click debug button again.
Wish it helps you!
Best Regards,
Kerry
hi @kerryzhou
Thanks for the information.
i forgot to mention tha i want to get debug over the 10 pin JTAG(J29),
i'm stalling the CMSIS-DAP firmware on the LPC-Link2,
i disconnect the on board debugger (J27 - J28) on xrt1020
i press th debug button and select the probe and im still getting the same error.
Hi @Irv95G ,
Ok, thanks for your updated information.
So, if your issue is solved, please help to mark the correct answer, just to close this case.
Any new issues, welcome to create the new case.
Best Regards,
Kerry