Hi There,
i.MX RT600 + murata Wi-Fi Module supports WHD driver or not?
I'm using SDK_2_10_1_EVK-MIMXRT685 and MCUXpressoIDE_11.4.1_6260
Thanks,
Hi @Sachin2
To the SDK_2_10_1_EVK-MIMXRT685, I find the wifi for the murata wifi module driver is removed, it just contains the nxp wifi module.
- One of the following Wi-Fi modules:
- Panasonic PAN9026 SDIO ADAPTER
- AzureWave AW-NM191NF-uSD + uSD to SD adapter
- AzureWave AW-AM457-uSD + uSD to SD adapter
- AzureWave AW-CM358-uSD + uSD to SD adapter
Even to the old SDK SDK_2.9.0_EVK-MIMXRT685 which contains the murrata module, i search the project, and didn't find the WHD driver, so maybe you need to port it by yourself, and refer to the cypress porting information:
https://infineon.github.io/wifi-host-driver/html/index.html
More details about the murrata, please contact cypress, thanks.
Best Regards,
Kerry