In the newly released documentation for the IMX RT1050, the LCD resolution is stated as being 800 x 480 WXGA in the datasheet. But on the overview page of your website the resolution is stated as being WXGA 1366 x 768. Which is correct?
解決済! 解決策の投稿を見る。
Hi,
The maximum resolution supported for the i.MX RT 1050 is 1366 x 768. But the resolution 800 x 480 display better. Both are OK. If you have any questions you can continue contact me.
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
I have a question about display resolution.
I want to drive a 1280x800 pixel LCD(fclk=71MHz) at 60Hz on the iMXRT1052.
Is it possible?
If possible, please provide example parameters.
Hi,
Is there any reply to this question?
As seeing in the reference manual there is no limit in the LCDIF_TRANSFER_COUNT field, and taking a look at the reference manual chapted of the Enhanced LCD Interface I haven't found any limitation, at least in the overview an functional Description.
Please someone reply, thank you.
Hi,
The maximum resolution supported for the i.MX RT 1050 is 1366 x 768. But the resolution 800 x 480 display better. Both are OK. If you have any questions you can continue contact me.
Have a great day,
Rita
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------