IMRT1176 Boot from flexspi1 secondary pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMRT1176 Boot from flexspi1 secondary pins

916件の閲覧回数
wangdabing
Contributor I

Hello nxp support ,

      In our project ,we  use imxrt1176 flexspi1 secondary pin group to connect a winbond  W25Q128FVSIG flash , but i can not boot ,every power on , the mcu enters serial download mode . i have burned the BT_FUSE_SEL ,SECONDARY GROUP , and i have got the rom log  by blhost  as follows,

wangdabing_1-1649233045890.pngwangdabing_2-1649233060333.png

 

and the FDCB i used as follows:

wangdabing_3-1649233128424.pngwangdabing_4-1649233139148.png

wangdabing_5-1649233188852.png

 

タグ(1)
0 件の賞賛
返信
3 返答(返信)

903件の閲覧回数
wangdabing
Contributor I

please to see the attachement for schemetic .and  also help me to check the sdram part of the schemetic. 

0 件の賞賛
返信

900件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply and clarification.
Firstly, after going through the schematic, I don't find any error with the QSPI connection.

Next, please follow the figure to check the eFuse setting.

jeremyzhou_0-1649298001540.png
Lastly, I'd like to suggest you use the MCUBootUtilitytool for testing.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 件の賞賛
返信

909件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Before giving some advice, I was wondering if you can share the schematic of the customize board.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信