How to flash two binary at a time durring production time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to flash two binary at a time durring production time

1,195件の閲覧回数
karthik1
Contributor I

Hi,

1) how to flash two binary files at a time at different location( custom bootloader (0x70100000) and application program(0x70000000)) location.   Note : Application is XIP  header enabled

2) or How to merge two binary file  into one file in different location3) 

Thanks and regards 

Karthik  N E

ラベル(2)
0 件の賞賛
返信
1 返信

1,115件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi karthik NE

 Please check these information which may useful to you:

1. Download AN12255

https://www.nxp.com/docs/en/application-note/AN12255.pdf 

Chapter 3.2.2. Programming multiple firmware to flash by MFGTool

2. About the merge, please check the following link

How to merge two s19 files to one file? 

Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信